cancel
Showing results for 
Search instead for 
Did you mean: 

"Port Open and try to configure the board"

EBerg.2
Associate II

Hello!

I am having trouble when connecting STM32 to Motor Pilot. I am using F302R8 control board and IHM07M1 as power board. I can see the port in Decive Manager and it says it is port COM5, but when I connect through COM5 from Motor Pilot I get the message "Port Open and try to configure the board" and I am unable to do anything at all in Motor Pilot. I have no clue what this means.

Regards,

Emelie

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
EBerg.2
Associate II

I have configurated the board as the manual says, the message is still there. USART2 is set in the "Connectivity"-category and MotorControl is set in the "Middelware"-category (maybe this is the problem?).

Muthanna
Associate III

I'm facing the same problem on EVSPIN32F02Q1S1.

The Motor Pilot Software says Port Open and try to configure the board when I click on connect.

@EBerg.2​ I don't think there's a problem with the MX Configuration. I think something is occupying the COM Port.

I'm stuck, not able to find answers anywhere.

Muthanna
Associate III

Hi @EBerg.2​ 

Didn't take long.

I was using the wrong baud rate aka "Speed" adj to Connect button.

The error isn't user friendly.

The correct speed fixed it

Regards,

Vineeth

THöfl.1
Associate III

Hi in my case i changed the boudrate to115200 and now it works well. LG Thomas

SujaySingh
ST Employee

Check the no. of shunts for which you have configured the IHM07M1 w.r.t code generation, & update the STLink through UTILITY.