2024-09-05 04:23 AM
i'm using Stm-Cube ide version 1.15.0 and getting this error when trying to flash the firmware.
2024-09-05 05:40 AM
Can you connect using the standalone STM32CubeProgrammer program?
What does test.elf do? If it goes into low power modes, or re-initialized SWD pins, or erases FLASH, this will cause issues with debug.
Is this a known good ST board or custom hardware?