Question about the RTC of STM32F103
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2013-05-07 6:29 AM
Posted on May 07, 2013 at 15:29
We're using RTC as a timer to wakeup STM32F103 from stop mode frequently, I'm quite confused on the descriptions in RM0008
1. what's the difference between RTC_IRQHandler and RTCAlarm_IRQHandler? If an alarm comes, both irq called? Is there a EXTI17_IRQHanlder?2. do I must clear all of EXTI_Line17, PWR_FLAG_WU, RTC_IT_ALR in some irq handler? what's the actual physical connection between the components that these registers reside on (plz help to explain based on Figure 179 in RM0008)?Thanks a lot! #rtc #stm32f1
Labels:
- Labels:
-
RTC
-
STM32F1 Series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0