cancel
Showing results for 
Search instead for 
Did you mean: 

Query on STM32G473CEU3

PY.1
Associate II

Hi,

We are using STM32G473CEU3 in our design

We have a situation that when MCU is powered off, 3.3V appears on one of the IO pins from an external circuit with 2mA of sourcing. Will this damage the MCU or is it ok?

1 REPLY 1
TDK
Guru

Per the datasheet, a voltage of 3.3V on a pin when VDD = 0 will not damage the chip. No current will be injected if the voltage is only 3.3V.

TDK_0-1723032578962.png

 

If you feel a post has answered your question, please click "Accept as Solution".