cancel
Showing results for 
Search instead for 
Did you mean: 

QUAD-SPI too busy!

Albi G.
Senior

Hi guys,

i am using the QuadSPI periphery to interface with a FPGA. I am in need of raw throughput with alternating write and read cycles of some number of bytes. I am just concept-prooving right now.

Since QUADSPI->CCR is not allowed to be modified when BUSY==1 the busy flag effectively limits the command rate - which is useful since i obviously need to wait to finish a a command before sending the next one.

My configuration is:

  • 4 bit wide Instruction
  • Skip directly to 4bit wide Data-transfer
  • Min CS-High time = 0 (1 cycle)
  • IndirectRead / IndirectWrite mode, no DMA for now.

Now, unfortunately the BUSY flag is rather lame and it takes exactly 6-7 clocks after CS rises that the BUSY flag clears. That is really **** ** the achievable command rate!

With 6-7 clocks, i mean periphery-clocks after the prescaler. (@1MHz SPI clock, the BUSY-signal is 1 for 6µs after CS rises. If 10MHz is used, then its 0.6us)

What i dont understand is, that this behavior makes the minimum CS-high setting kind of useless. (i never achieve a scenario where CS is less than 6 cycles high in-between commands)

This holds true for consecutive reads, consecutive writes, and alternating read-write.

What could go wrong ??

This is my example code. Not using the library, but my code hopefully reads kind of intuitively...


_legacyfs_online_stmicro_images_0693W000001qTAI.png

Measured though my Debug-GPIO: 16.7µs from Command start to BUSY=0

Chip select Low for 11µs

Give me a faster BUSY, please :(

BTW: i also get the same behavior if i configure the QSPI differently:

  • skip Instruction
  • Send one byte address
  • skip directly to Data

== Same timing(-problems)

thanks

This discussion is locked. Please start a new topic to ask your question.
21 REPLIES 21

One of the other potential pitfalls of using the QSPI/FMC external interfaces for things like FIFO's or state-machines is that the core/peripheral can do funny things with unaligned access, bursts access, speculative reads, and reads which are abandoned and retried.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Arnon
Associate III

Those "funny things" is what made go and look at the CS and clock.

I would never imagine that clock could start before CS goes down....