2016-09-26 6:20 AM
Hi.
I have a project working with a STM32F2/F4. I want to upgrade this project a bit, adding a CPLD/FPGA to do certain tasks that actually is doing the micro.We have done a small test and it worked with a SPI and a CPLD... but we would like it faster.We have the option to send from several SPIs or use QUADSPI, logically QUADSPI would be better, but reading the docs it seems oriented to work with Flash Memories, I dont know if it is possible to transmit your own data.Is it possible to use QUADSPI like SPI, just using DMA and transfering a long block of data to the output, sending hi/low nibble alternatively?.Best Regards.2016-09-26 8:38 AM
Not sure about writing. Reading would seem to require you just to emulate enough of the support FLASH/EPROM protocol.
Could you use an SDIO based interface? How about a condensed FSMC one? Inbound parallel data, look at DCMI2016-09-27 1:06 AM
2016-09-27 1:35 AM
It is very interesing the last document. It is probably easier that i tough, at least if i use the Flexible Frame Format
http://www.st.com/content/ccc/resource/technical/document/application_note/group0/b0/7e/46/a8/5e/c1/48/01/DM00227538/files/DM00227538.pdf/jcr:content/translations/en.DM00227538.pdfChapter 2.1 (page 13/87) It sends a instruccion byte, then 4 bytes address, a dumy byte and the info.Ignoring the first n clocks after a transfer (2 x 1+4+1 = 12) i would access to the data. I would make it a bit more ''intelligent'' processing at least the instruction byte (i would use 2 instruccions, one for configuring, and another for normal process).If i'm not wrong this would work.2016-09-27 5:07 AM
Without putting any effort into PCB routing, I'm getting around 6.5MHz write speed between an F407 and an FPGA using the FSMC with separated 16-bit address and data buses, i.e. over 100Mbps of data throughput. There's no mucking around with the peculiarities of a peripheral like SDIO or QSPI, (SDIO is quite fiddly; I haven't used QSPI so can't comment), and it scales from 1-byte operations to bulk data via memory-to-memory DMA transfers.
2016-09-28 7:54 AM
Use block RAM inside of the CPLD/FPGA to create dual Port SRAM, attach the STM32 via FSMC in SRAM or i80/LCD mode, fastest connection possible and easy to use.
Best regards,
Markus.