2016-09-28 6:29 AM
I amusing the example program to run a single PWM and it works. All I am trying to do is run the CPU at a slower speed to conserve power. If I run it at 8Mhz with a pll setting of less the times 6 (so 48Mhz), the HRTIM will always timeout during calibration.
I have set the sysTick to give 1ms interrupts.
Is this a limitation of the HRTIM or is there something I can do?
2016-09-28 7:29 AM
Hello,
Have a look to this
''HRTIM cookbook''. It may help you.
RegardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.