cancel
Showing results for 
Search instead for 
Did you mean: 

PWM Output on STM32F2XX (Solved)

th2
Associate
Posted on February 02, 2012 at 14:30

Greetings,

I am currently toying around with the KEIL MCBSTM32F200 Evaluation Board

(the STM32F207VG uC) and have run into some problems with the PWM output.

I want a simple PWM-signal on TIM1, Channel1 (PA8 for STM32F205&207) using

the standard peripheral library for STM32Fxx.

The code below is a mix from the different examples from the standard

peripheral library examples for PWM, and I'm sure something critical is

missing.

After initializing, all TIM1 registers looks ''ok'' (as far as I can tell, the

timer is a bit too advanced for me...) and the TIM1_CNT register is counting

up and resetting.

When connecting the oscilloscope to PA8, all I get is a steady 3.3V signal,

no PWM.

What am I missing here? It's quite frustrating since all other peripherals

I'm using are working fine. Thanks in advance.

(code also at

http://pastebin.com/yUmZbXUL

: http://pastebin.com/yUmZbXUL)

&sharpinclude ''stm32f2xx.h''

&sharpinclude ''stm32f2xx_gpio.h''

&sharpinclude ''stm32f2xx_rcc.h''

&sharpinclude ''stm32f2xx_tim.h''

&sharpinclude ''system_stm32f2xx.h''

/****************************************************************************/

void main(void) {

TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;

TIM_OCInitTypeDef TIM_OCInitStructure;

GPIO_InitTypeDef GPIO_InitStructure;

uint16_t period;

uint16_t pulse;

/* Initialize clock - defined in system_stm32f2xx.h */

SystemInit();

/* Compute the value for the ARR register to have a period of 20 KHz */

period = (SystemCoreClock / 20000 ) - 1;

/* Compute the CCR1 value to generate a PWN signal with 50% duty cycle */

pulse = (uint16_t) (((uint32_t) 5 * (period - 1)) / 10);

/* GPIOA clock enable */

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);

/* Initialize PA8, Alternative Function, 100Mhz, Output, Push-pull */

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ;

GPIO_Init(GPIOA, &GPIO_InitStructure);

GPIO_PinAFConfig(GPIOA, GPIO_PinSource8, GPIO_AF_TIM1);

/* TIM1 clock enable */

RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1 , ENABLE);

/* Timer Base configuration */

TIM_TimeBaseStructInit(&TIM_TimeBaseStructure);

TIM_TimeBaseStructure.TIM_Prescaler = 0;

TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

TIM_TimeBaseStructure.TIM_Period = period;

TIM_TimeBaseStructure.TIM_ClockDivision = 0;

TIM_TimeBaseStructure.TIM_RepetitionCounter = 0;

TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure);

/* Channel 1 output configuration */

TIM_OCStructInit(&TIM_OCInitStructure);

TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM2;

TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

TIM_OCInitStructure.TIM_Pulse = pulse;

TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_Low;

TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Set;

TIM_OC1Init(TIM1, &TIM_OCInitStructure);

/* TIM1 counter enable */

TIM_Cmd(TIM1, ENABLE);

/* TIM1 Main Output Enable */

TIM_CtrlPWMOutputs(TIM1, ENABLE);

/* forever... */

while (1) {

__asm(''nop'');

}

}

#stm32f2xx-pwm-tim1
This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Posted on July 18, 2016 at 17:47

This should work for a F2/F4 part with TIM1_CH1 on PE9

// STM32 PWM (TIM1 CH1 PE.09) STM32F4 Discovery - sourcer32@gmail.com
#include ''stm32f4_discovery.h''
/**************************************************************************************/
void RCC_Configuration(void)
{
/* --------------------------- System Clocks Configuration -----------------*/
/* TIM1 clock enable */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE);
/* GPIOE clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOE, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/*-------------------------- GPIO Configuration ----------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOE, &GPIO_InitStructure);
/* Connect TIM1 pins to AF */
GPIO_PinAFConfig(GPIOE, GPIO_PinSource9, GPIO_AF_TIM1);
}
/**************************************************************************************/
void TIM1_Configuration(void)
{
TIM_OCInitTypeDef TIM_OCInitStructure;
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
uint16_t Period;
Period = 1000000 / 20000; // 20 KHz for 1MHz prescaled
/* Time base configuration */
TIM_TimeBaseStructure.TIM_Prescaler = (SystemCoreClock / 1000000) - 1; // Get clock to 1 MHz on STM32F2/F4
TIM_TimeBaseStructure.TIM_Period = Period - 1;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_RepetitionCounter = 0;
TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure);
/* Enable TIM1 Preload register on ARR */
TIM_ARRPreloadConfig(TIM1, ENABLE);
/* TIM PWM1 Mode configuration */
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCInitStructure.TIM_Pulse = Period / 2; // 50%
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Reset;
TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Disable;
TIM_OCInitStructure.TIM_OCNPolarity = TIM_OCNPolarity_High;
TIM_OCInitStructure.TIM_OCNIdleState = TIM_OCNIdleState_Reset;
/* Output Compare PWM1 Mode configuration: Channel1 PA.08 */
TIM_OC1Init(TIM1, &TIM_OCInitStructure);
TIM_OC1PreloadConfig(TIM1, TIM_OCPreload_Enable);
/* TIM1 Main Output Enable */
TIM_CtrlPWMOutputs(TIM1, ENABLE);
/* TIM1 enable counter */
TIM_Cmd(TIM1, ENABLE);
}
/**************************************************************************************/
int main(void)
{
RCC_Configuration();
GPIO_Configuration();
TIM1_Configuration();
while(1); // Don't want to exit
}
/**************************************************************************************/
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* User can add his own implementation to report the file name and line number,
ex: printf(''Wrong parameters value: file %s on line %d

'', file, line) */
/* Infinite loop */
while (1)
{
}
}
#endif
/**************************************************************************************/

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..