2007-09-23 10:58 AM
programming support
2011-05-17 03:15 AM
Have you seen it? Elnec has released full programming support for STM32F devices - see
http://www.elnec.com/content/?action=show_file&file=sw/pg4u_ver_beta.txt
Enjoy it :)2011-05-17 03:15 AM
Thank You opijozko :)
The BeeHive from ELNEC programmers provide sites for programming up to 4 devices concurrently or sequentially. BeeProg is the Elnec single-site programmer featuring USB to host-PC connection, and control of multiple BeeProg programmers from a single PC. Both are supported by a range of interchangeable sockets for all packages in the growing range of supported microcontrollers. Elnec programmers support a wide range of other ST devices including the STR9 ARM996Eâ„¢ core-based devices, the STR7 ARM7TDMIâ„¢ core-based devices, and our ST7 family of 8-bit microcontrollers.