2007-09-23 11:26 AM
32kHz clock
2011-05-17 3:15 AM
What are the recommended CL and maximum ESR for a 32kHz crystal, on the STM32F103RB?
For example, is CL=12.5pF and ESR=35kOhm okay?2011-05-17 3:15 AM
Dear espresso_solo,
Generally these values depend on the Quartz manufacturers, you can refer to our Application Notehttp://www.st.com/stonline/products/literature/an/13675.pdf
and also to the STM32 Datasheets or , Section : Operating conditions then then External clock source characteristics For more details. With best regards, STOne-32 [ This message was edited by: STOne-32 on 24-09-2007 00:19 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.