2021-08-28 4:08 AM
Hello,
I am using STM32F746BGT6
I am trying for LED toggling.
I am using cube programmer for downloading hex. I am facing verification issue, but download was successful. After download complete, i reset my controller. But my toggle logic is not working. when i am doing debug, the code always go to hard fault handler function.
Thanks
Manikandan D
2021-08-28 5:29 AM
Then you're going to need to debug more.
Probably goes to the Hard Fault handler in both cases. Have it output actionable data.
Perhaps start by looking at the faulting instructions and registers are the fault, understand what was happening there.
Writing to a bad pointer, enabling an interrupt, etc.
If it doesn't make it to main(), start the debugger earlier, uncheck "run to main" type options and stepping in code.
Hard Fault have been covered here very many times..
2021-08-28 10:48 AM
If verification was not successful, then likely it did not download successfully either.
2021-08-30 12:22 AM
Hello, here i attached one screenshot. In my debug section i find out the issue in startup file. when debug is start, bl systemInit done successfully, but after coming to bl __libc_init_array then it's directly going to HardFaultHandler function. I don't know what's happening here .
Thanks
Manikandan D