2014-12-16 03:31 AM
Hi i'm an italian student and i have to use IAR (for ARM) for c/c++ programming to control the stm32f401.
I'm trying to run a simple example program but i get always this error (i'm running windows 7 and i've tried it on different machines):Tue Dec 16, 2014 12:13:45: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.0\arm\config\debugger\ST\STM32F4xx.dmac Tue Dec 16, 2014 12:13:45: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.0\arm\config\flashloader\ST\FlashSTM32F4xxx.mac Tue Dec 16, 2014 12:14:00: Fatal error: Failed to search for probes, ensure that the USB drivers are installled. Session aborted! Tue Dec 16, 2014 12:14:00: Failed to load flash loader: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.0\arm\config\flashloader\ST\FlashSTM32F401x.flash Thanks. #iar-workbenc