2013-12-05 7:48 AM
2013-12-05 8:47 AM
the microcontroller hangs.
Hangs where? If you understand where, you might be able to determine why.
I'm
using the
CAN1
and
CAN2
controller
micorcontrolador
STM32F207IG
.but I have
the following problem
:Both controllers
are communicating
normally
,but when
the communication cable
from the controller
microcontroller
1
is
open
latch
.Could someone help
me on this
problem,
is it possible to
enable and
disable the
CAN controller
??Thank you.
The
following
code
:
I'm
using the
CAN1
and
CAN2
controller
micorcontrolador
STM32F207IG
.but I have
the following problem
:Both controllers
are communicating
normally
,but when
the communication cable
from the controller
microcontroller
1
is
open
latch
.Could someone help
me on this
problem,
is it possible to
enable and
disable the
CAN controller
??Thank you.
The
following
code
:
I'm
using the
CAN1
and
CAN2
controller
micorcontrolador
STM32F207IG
.but I have
the following problem
:Both controllers
are communicating
normally
,but when
the communication cable
from the controller
microcontroller
1
is
open
latch
.Could someone help
me on this
problem,
is it possible to
enable and
disable the
CAN controller
??Thank you.
The
following
code
:
I'm
using the
CAN1
and
CAN2
controller
micorcontrolador
STM32F207IG
.but I have
the following problem
:Both controllers
are communicating
normally
,but when
the communication cable
from the controller
microcontroller
1
is
open
latch
.Could someone help
me on this
problem,
is it possible to
enable and
disable the
CAN controller
??Thank you.
The
following
code
:2013-12-05 9:03 AM
Lock in the following function:
if((CAN_receive (1, &msg_rece, 15) == CAN_OK)) { if(msg_rece.id==40) { Rece_CAN1 = msg_rece.data[0]; }}else {com_CAN_1=0, Rece_CAN1=0;}