Problems getting sd-link to flash - STM32746G-DISCO_Demo_V1.1.0.hex
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-07-18 5:39 AM
I'm having problems getting sd-link to flash. I've no tried it on linux, a mac, and a Raspberry Pi. The Raspberry Pi at least manages to read it!
I'd just like to flash the demo STM32746G-DISCO_Demo_V1.1.0.hex correctly - once that works, I'm hoping flashing embedded code will be easy!
What am I doing wrong?I've got the link up:st-util
2016-07-18T14:14:21 INFO src/common.c: Loading device parameters....
2016-07-18T14:14:21 INFO src/common.c: Device connected is: F7 device, id 0x10016449
2016-07-18T14:14:21 INFO src/common.c: SRAM size: 0x50000 bytes (320 KiB), Flash: 0x100000 bytes (1024 KiB) in pages of 2048 bytes
2016-07-18T14:14:21 INFO src/gdbserver/gdb-server.c: Chip ID is 00000449, Core ID is 5ba02477.
2016-07-18T14:14:21 INFO src/gdbserver/gdb-server.c: Chip clidr: 09000003, I-Cache: off, D-Cache: off
2016-07-18T14:14:21 INFO src/gdbserver/gdb-server.c: cache: LoUU: 1, LoC: 1, LoUIS: 0
2016-07-18T14:14:21 INFO src/gdbserver/gdb-server.c: cache: ctr: 8303c003, DminLine: 32 bytes, IminLine: 32 bytes
2016-07-18T14:14:21 INFO src/gdbserver/gdb-server.c: D-Cache L0: 2016-07-18T14:14:21 INFO src/gdbserver/gdb-server.c: f003e019 LineSize: 8, ways: 4, sets: 32 (width: 10)
2016-07-18T14:14:21 INFO src/gdbserver/gdb-server.c: I-Cache L0: 2016-07-18T14:14:21 INFO src/gdbserver/gdb-server.c: f007e009 LineSize: 8, ways: 2, sets: 64 (width: 11)
2016-07-18T14:14:21 INFO src/gdbserver/gdb-server.c: Listening at *:4242...
I get these errors from st-info:st-info --chipid
[!] send_recv send request failed: LIBUSB_ERROR_IO
[!] send_recv STLINK_GET_CURRENT_MODE
[!] send_recv send request failed: LIBUSB_ERROR_IO
[!] send_recv STLINK_GET_CURRENT_MODE
[!] send_recv send request failed: LIBUSB_ERROR_IO
[!] send_recv STLINK_DEBUG_ENTER
0x0000
[!] send_recv send request failed: LIBUSB_ERROR_IO
[!] send_recv STLINK_JTAG_WRITEDEBUG_32BIT
Which doesn't look good.I seem to be able to read from flash memory, but not write to it:$st-flash read out.bin 0x8000000 1048576
2016-07-18T14:37:28 INFO src/common.c: Loading device parameters....
2016-07-18T14:37:28 INFO src/common.c: Device connected is: F7 device, id 0x10016449
2016-07-18T14:37:28 INFO src/common.c: SRAM size: 0x50000 bytes (320 KiB), Flash: 0x100000 bytes (1024 KiB) in pages of 2048 bytes
$/media/Ada/stlink.git♯ st-flash write out.bin 0x8000000 1048576
2016-07-18T14:37:48 WARN src/sg.c: Failed to find an stlink v1 by VID:PID
2016-07-18T14:37:48 ERROR src/sg.c: Could not open stlink device
Any suggestions? #programming #problem #flash #stm32746g-discovery- Labels:
-
Flash
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-07-18 6:42 AM
> I've no tried it ...
I assume you mean ''now
tried it ...'' - would have a significant influence on the meaning.> I've no tried it on linux, a mac, and a Raspberry Pi. The Raspberry Pi at least manages to read it!Assuming you are running a Linux OS on the Raspberry, it should work on a ''normal'' Linux, too. Perhaps just an issue of missing user permissions ? Using Crossworks on Linux (supports the ST-Link), I need to add rule files to /etc/udev/rules.d, to allow others than root access to such USB devices.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-07-18 6:45 AM
BTW, forgot to mention that the ST-Link V2.1 has another product ID than the older V2.
So earlier/older udev permission rules do not apply to this new version ...- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-07-18 7:06 AM
Yes, 'now tried it' - you're right.
I've got the rules set to mode 0666 - so that shouldn't be the problem.This is what puzzles me:st-flash read out.bin 0x8000000 1048576
2016-07-18T16:00:54 INFO src/common.c: Loading device parameters....
2016-07-18T16:00:54 INFO src/common.c: Device connected is: F7 device, id 0x10016449
2016-07-18T16:00:54 INFO src/common.c: SRAM size: 0x50000 bytes (320 KiB), Flash: 0x100000 bytes (1024 KiB) in pages of 2048 bytes
# st-flash write out.bin 0x8000000 1048576
2016-07-18T16:01:19 WARN src/sg.c: Failed to find an stlink v1 by VID:PID
2016-07-18T16:01:19 ERROR src/sg.c: Could not open stlink device
It is happy to read - but, suddenly, can't write.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-07-18 7:17 AM
> It is happy to read - but, suddenly, can't write.
Honestly, I don't know. Haven't tried the st-link tools since the (in-)famous vl-discovery times. I always used the boards from within Crossworks. Perhaps it's an issue with the tool itself, and the new V2.1 hardware ? Wine/Windows as last resort ?- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-07-18 7:57 AM
Hi brooks.peter.001,
Try to upgrade the ST-Link firmware to V2-1 version through this Link through the ST-Link utility. -Hannibal-- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-07-18 10:22 PM
That requires Windows - and you could flash you application directly from the ST-Link utility then.