cancel
Showing results for 
Search instead for 
Did you mean: 

Problems found in STM32F746NG USER MANUAL

NEERAJ GUPTA
Associate II
Posted on July 20, 2017 at 12:55

Refering to page no 167 in en.DM00124865.pdf  which is available as STM32F746NG USER MANUAL. 

These are following typo errors are found as follows:

Bit 10 ADC3EN: ADC3 clock enable

This bit is set and cleared by software.

0: ADC3 clock disabled

1: ADC3 clock disabled

Bit 9 ADC2EN: ADC2 clock enable

This bit is set and cleared by software.

0: ADC2 clock disabled

1: ADC2 clock disabled

Bit 8 ADC1EN: ADC1 clock enable

This bit is set and cleared by software.

0: ADC1 clock disabled

1: ADC1 clock disabled

Please! correct this also as soon as possible.

1 REPLY 1
Imen.D
ST Employee
Posted on July 20, 2017 at 14:51

Hi

GUPTA.NEERAJ

,

I confirm these typo errors.

This is already noted internally to be correct in the coming release of RM0

Thanks and Best Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen