2017-07-20 3:55 AM
Refering to page no 167 in en.DM00124865.pdf which is available as STM32F746NG USER MANUAL.
These are following typo errors are found as follows:
Bit 10 ADC3EN: ADC3 clock enable
This bit is set and cleared by software.0: ADC3 clock disabled1: ADC3 clock disabledBit 9 ADC2EN: ADC2 clock enableThis bit is set and cleared by software.0: ADC2 clock disabled1: ADC2 clock disabledBit 8 ADC1EN: ADC1 clock enableThis bit is set and cleared by software.0: ADC1 clock disabled1: ADC1 clock disabledPlease! correct this also as soon as possible.
2017-07-20 5:51 AM
Hi
GUPTA.NEERAJ
,I confirm these typo errors.
This is already noted internally to be correct in the coming release of RM0
Thanks and Best Regards
Imen