cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with stm32l4 tim16

Rsu.1
Associate II

I have use stm32l412cbt6 PB9 to input function and i can get the input data,then i configure PB9 to alternate function GPIO_AF14_TIM16 and i can not get the input data.Under the same configuration,PA3 alternate function GPIO_AF1_TIM2 can get the input data.Please give me some advice.

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11

Hello @waclawek.jan ,

This typo is fixed in DS12469 Rev 9.

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks, Kaouthar.

Jan