cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with stm cubeMX and keil

antonio23
Associate II
Posted on February 10, 2015 at 09:46

Hi to all,  i use CubeMX and Keil 5.12  with Stm Nucleo, STM32L152RE, all work well.

Yesterday  I upgrade the CubeMX to 4.6 version,  later this upgrade i have this error:

--- The Project references devices, files or libraries that are not installed Download and Install

Third Party Device Support for ''STMicroelectronics :STM32L125RE'' (Device not included in Legancy Device Satabases)---

i  upgrade Keil to the 5.13 version,  in Pack Install i uninstall and later install the packeg for StM32L152 but don't work.

if  I open blink example all work well, if i use other  easy example  all work well, but if i use the code of CubeMx i have this message error.

can you help me?

best regards

Antonio
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
stm32cube-t
Senior III
Posted on July 01, 2015 at 11:40

Hello we are unable to reproduce your issue:

Trying to reproduce: using a project generated by MX but with keil::STM32L1xx_DFP pack already installed, everything goes well and no error message appears. 

Remove the keil pack and try again: the error message appears asking to install the correspanding pack.

Your issue is likely due to the fact the keil pack is not properly installed/missing.

Best regards