Problem with SPI transmission on G071
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-22 3:59 AM
Hi,
I am having problems sending a part of an array with SPI. It is no problem to send 4 Bytes from the beginning of the array, but if I want to send 4 Bytes from another starting position (for example: start from tmp[1]) it does not work. In this case I can see on the oscilloscope that the command and the address are transmitted and after that comes nothing.
Any ideas??
uint8_t tmp[6] = {6,1,6,1,5,5};
uint8_t *ptr = &tmp[0];
uint8_t *ptr2;
uint8_t command = 0, len=4, address = 0x07;
ptr2 = &tmp[1];
HAL_GPIO_WritePin(SPISSN_GPIO_Port, SPISSN_Pin, RESET);
// Write & Length
command = 0x80 | (len & 0x7F);
HAL_SPI_Transmit(&hspi2, (uint8_t*)(&command), 1, 100);
//address
HAL_SPI_Transmit(&hspi2, (uint8_t*)(&address), 1, 100);
//send "len" bytes of data
HAL_SPI_Transmit(&hspi2, tmp, len, 100); //ok
HAL_SPI_Transmit(&hspi2, ptr, len, 100); //ok
HAL_SPI_Transmit(&hspi2, ptr2, len, 100); //NOT ok
HAL_GPIO_WritePin(SPISSN_GPIO_Port, SPISSN_Pin, SET);
Kind regards,
Bernd
- Labels:
-
SPI
-
STM32G0 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-22 4:30 AM
When you send ptr2, do you have a clock signal and the data is bad or does nothing happen at all?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-22 4:42 AM
First try with 8 bit mode spi and 8 bit dma transfer to make sure it is not a odd memory alignment issue.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-22 6:24 AM
Clock signal is ok until address is sent, after this nothing happens.
I am using 8 bit spi mode.
Strange is, that nothing happens after the address, no wrong values.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-22 12:54 PM
This is a documented behaviour - if you provide a halfword-unaligned address and request to trnasfer more than a byte, Cube/HAL attempts to read a halfword from the memory and that leads to hardfault on Cortex-M0/M0+.
This is from CubeF0 but I guess the same you'll find in CubeG0 too:
(#) In case more than 1 byte is requested to be transferred, the HAL SPI uses 16-bit access for data buffer.
But there is no support for unaligned accesses on the Cortex-M0 processor.
So, if the user wants to transfer more than 1 byte, it shall ensure that 16-bit aligned address is used for:
(##) pData parameter in HAL_SPI_Transmit(), HAL_SPI_Transmit_IT(), HAL_SPI_Receive() and HAL_SPI_Receive_IT()
(##) pTxData and pRxData parameters in HAL_SPI_TransmitReceive() and HAL_SPI_TransmitReceive_IT()
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-25 12:41 AM
It seems to be the same behaviour, but it is not documented. As a workaround, I will copy the data into a temp. array and send the data from this array.
Kind regards,
Bernd