2013-04-26 2:57 PM
Hello,
I'm astudent of computer engineering, I'm trying to interface a STM32F0_Discoverycard with an LIS3LV02DQ accelerometer using the SPI protocol, but I'm havingtrouble with the initialization of the pins of the STM32F0_Discovery related tothe SPI protocol. Below I attach the code I used
void
SPI2_Init(
void
)
{
//SPI & GPIO struct
SPI_InitTypeDef
SPI_InitStructure;
GPIO_InitTypeDef
GPIO_InitStructure;
RCC_APB2PeriphClockCmd(RCC_APB1Periph_SPI2,
ENABLE
);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB| RCC_AHBPeriph_GPIOD,
ENABLE
);
//MISO, MOSI,CLOCK
GPIO_InitStructure.
GPIO_Pin
= GPIO_Pin_13|GPIO_Pin_14 |GPIO_Pin_15;
GPIO_InitStructure.
GPIO_Mode
=
GPIO_Mode_AF
;
GPIO_InitStructure.
GPIO_OType
=
GPIO_OType_PP
;
GPIO_InitStructure.
GPIO_PuPd
=
GPIO_PuPd_DOWN
;
GPIO_InitStructure.
GPIO_Speed
=GPIO_Speed_50MHz;
GPIO_Init(GPIOB,&GPIO_InitStructure);
GPIO_PinAFConfig(GPIOB,GPIO_PinSource13, GPIO_AF_0);
GPIO_PinAFConfig(GPIOB,GPIO_PinSource14, GPIO_AF_0);
GPIO_PinAFConfig(GPIOB,GPIO_PinSource15, GPIO_AF_0);
//CS
GPIO_InitStructure.
GPIO_Pin
= GPIO_Pin_12;
GPIO_InitStructure.
GPIO_Mode
=
GPIO_Mode_OUT
;
GPIO_InitStructure.GPIO_OType
=
GPIO_OType_PP
;
GPIO_InitStructure.
GPIO_PuPd
=
GPIO_PuPd_UP
;
GPIO_InitStructure.
GPIO_Speed
=GPIO_Speed_50MHz;
GPIO_Init(GPIOB,&GPIO_InitStructure);
//SPI2configuration
SPI_I2S_DeInit(SPI2);
SPI_StructInit(&SPI_InitStructure);
SPI_InitStructure.
SPI_BaudRatePrescaler
=SPI_BaudRatePrescaler_2;
SPI_InitStructure.
SPI_CPOL
= SPI_CPOL_Low;
SPI_InitStructure.SPI_CPHA
=SPI_CPHA_2Edge;
SPI_InitStructure.SPI_CRCPolynomial
= 7;
SPI_InitStructure.
SPI_DataSize
=SPI_DataSize_8b;
SPI_InitStructure.
SPI_Direction
=SPI_Direction_2Lines_FullDuplex;
SPI_InitStructure.
SPI_FirstBit
=SPI_FirstBit_MSB;
SPI_InitStructure.
SPI_Mode
= SPI_Mode_Master;
SPI_InitStructure.
SPI_NSS
= SPI_NSS_Soft;
SPI_Init(SPI2,&SPI_InitStructure);
SPI_Cmd(SPI2,
ENABLE
);
}
Debuggingstep by step I noted that the fields of the struct SPI_InitStructure andGPIO_InitStructure are properly modified according to the values
​​
that I specified. The values
​​
contained in the registers GPIOB are changed
when the GPIO_Init function is performed , butthe registers of SPI2 are not affected when the SPI_Init function is invoked .I would ask if I am making mistakes in the settings or anything.
I also havea doubt on the SPI read Protocol of the accelerometer. In fact I would like toread the WHO_AM_I register, and in order to do this as first thing, I send abyte specifying the read command and the address of the register from which Iwant to read using the SPI_SendData8 function and then run the reading usingthe SPI_ReceiveData8 function. I would ask you if the procedure is correct.Here's the code I used.
uint8_t
who=NULL;
uint8_t
reg_send;
reg_send = 0x0F; //WHO_AM_Iregister address
reg_send |= 128;
while
(SPI_I2S_GetFlagStatus(SPI2,SPI_I2S_FLAG_TXE)==
RESET
);
SPI_SendData8(SPI2,reg_send);
while
(SPI_I2S_GetFlagStatus(SPI2,SPI_I2S_FLAG_RXNE)==
RESET
);
who=SPI_ReceiveData8(SPI2);
I want to informyou that I use the Atollic IDE.
Thanks inadvance for the help that you will give me.
Bestregards.