2013-04-26 1:54 PM
Hello,
I'm trying to count pulse on PB7 using timer TIM4 ch2. Everything is ok, but I'd like to reset CCR2 so I can start another measure. I tried with TIM_SetCompare2(TIM4, 0); but CCR2 isn't set to 0 after execution. Here's how I setup TIM4: GPIO_InitTypeDef GPIO_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; /* TIM4 clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE); /* GPIOB clock enable */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE); /* TIM4 chennel2 configuration : PB.07 */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ; GPIO_Init(GPIOB, &GPIO_InitStructure); /* Connect TIM pin to AF2 */ GPIO_PinAFConfig(GPIOB, GPIO_PinSource7, GPIO_AF_TIM4); /* Enable the TIM4 global Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = TIM4_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); TIM_TimeBaseStructure.TIM_Period = 65535; TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure); TIM_TIxExternalClockConfig(TIM4,TIM_TIxExternalCLK1Source_TI2,TIM_ICPolarity_Rising,0); //TI2FP2 /* TIM enable counter */ TIM_Cmd(TIM4, ENABLE); /* Enable the CC2 Interrupt Request */ TIM_ITConfig(TIM4, TIM_IT_CC2, ENABLE); Thanks, Simone2013-04-26 2:32 PM
The write goes to a shadow register, and this doesn't forward until the counter rolls (ie at update), the counter also needs to be clocked, as I recall.
If channel CC2 is configured as output: CCR2 is the value to be loaded in the actual capture/compare 2 register (preload value).It is loaded permanently if the preload feature is not selected in the TIMx_CCMR2 register (bit OC2PE). Else the preload value is copied in the active capture/compare 2 register when an update event occurs.
CNT holds the count, CCR2 is a latch and doesn't count.
2013-04-26 2:53 PM
Thank you very much for answer!
Problem solved by settingTIM_SetCounter(TIM4, 0); and waiting for the next pulse.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.