cancel
Showing results for 
Search instead for 
Did you mean: 

problem with programing aplication

Posted on November 27, 2015 at 09:26

Hi all,

I have a problem with programing STM32L15V.

I am using about 1m long connection to device from ST Link V2.

When I am using STM32 ST-LINK Utility (V3.7.0) there is no problem with connection/programing/erase.

When I try to use ST-LINK_CLI (V2.3.0) from command line I can not connect to microcontroler.

I have need to use CLI as I need to automate process using LabView.

Any idea ?

Br,

Lucas
2 REPLIES 2
Nesrine M_O
Lead II
Posted on November 30, 2015 at 12:43

Hi Lucas,

“When I try to use ST-LINK_CLI (V2.3.0) from command line I can not connect to microcontroler.�

You may ignored some parameters in your connect command, so it uses the default ones

try this -c SWD UR

-Syrine-

shahril rizal hassan
Associate II
Posted on October 12, 2017 at 03:56

Hi Lucas,

I working to automated the CLI process using labview also...can you share the labview vi to me?

Best regards,

Shahril