2020-07-28 5:17 AM
Hi,
I'm using the FLASH_Write function in order to save a table in a specific address. Once it is saved correctly I reset the board and try to change another address with the same function.
The problem is that the flash_write function works at the first try but once the reset is done, the flush_write crushes and give me this error "FLASHIF_WRITING_ERROR".
Does anyone know why it crushes in the second time after a reset ?
You may find the flash_write file attached to this post.
2020-07-28 5:47 AM
What chip?
Programming double words may not be supported on your chip for the voltage you have.
2020-07-28 6:22 AM
I'm using the STM32L476VG
I found out that the problem is actually coming from the Flash_Erase
uint32_t FLASH_If_Erase(uint32_t start)
{
uint32_t NbrOfPages = 0;
uint32_t PageError = 0;
FLASH_EraseInitTypeDef pEraseInit;
HAL_StatusTypeDef status = HAL_OK;
/* Unlock the Flash to enable the flash control register access *************/
HAL_FLASH_Unlock();
/* Get the number of page to erase */
NbrOfPages = (FLASH_START_ADRESS + FLASH_SIZE);
NbrOfPages = (NbrOfPages - start) / FLASH_PAGE_SIZE;
if(NbrOfPages > FLASH_PAGE_NBPERBANK)
{
pEraseInit.Banks = FLASH_BANK_1;
//pEraseInit.NbPages = NbrOfPages % FLASH_PAGE_NBPERBANK;
pEraseInit.NbPages = 32;
pEraseInit.Page = FLASH_PAGE_NBPERBANK - pEraseInit.NbPages;
pEraseInit.TypeErase = FLASH_TYPEERASE_PAGES;
status = HAL_FLASHEx_Erase(&pEraseInit, &PageError);
NbrOfPages = FLASH_PAGE_NBPERBANK;
}
if(status == HAL_OK)
{
pEraseInit.Banks = FLASH_BANK_2;
pEraseInit.NbPages = NbrOfPages;
pEraseInit.Page = FLASH_PAGE_NBPERBANK - pEraseInit.NbPages;
pEraseInit.TypeErase = FLASH_TYPEERASE_PAGES;
status = HAL_FLASHEx_Erase(&pEraseInit, &PageError);
}
/* Lock the Flash to disable the flash control register access (recommended
to protect the FLASH memory against possible unwanted operation) *********/
HAL_FLASH_Lock();
if (status != HAL_OK)
{
/* Error occurred while page erase */
return FLASHIF_ERASEKO;
}
return FLASHIF_OK;
}
When I use pEraseInit.NbPages = NbrOfPages % FLASH_PAGE_NBPERBANK; the Flash_Erase works fine, but it also erase the rest of the ship where I have stored other parameters. I only want to erase 32 pages so I have tried pEraseInit.NbPages = 32K; but it doesn't work