cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with FATFS File System on nucleo Board L152RE

babanthierry
Associate
Posted on October 14, 2015 at 16:03

Hi,

I would like to know if it's possible to use FATFS file system on a nucleo L152RE without using memory card.

I just want to use the flash of the nucleo board but i need to save some informations with three fields.

for example

name;telephone number;adress
1 REPLY 1
Posted on October 14, 2015 at 21:42

Not sure why that would even need a file-system. Can't you just develop an in-memory structure and write it too an unused upper flash memory sector?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..