Skip to main content
Dimitris Paraskevopoulos
Associate III
December 11, 2014
Question

Problem with CubeMX 4.5.0

Posted on December 11, 2014 at 17:28

I would like to point out the problems that I have encountered with CubeMX thus far.

I am trying to set up an SPI communication between an STM32F401RE Nucleo board (Master) and an mbed LPC1768. I tried using the CubeMX code generator and export it into Keil 5 but I couldn't load the program.

Even though I chose the correct board when trying to setup the code when the code was generated and loaded into Keil it reported a different Target name.

I tried to change the target options to the STM but it didn't work.

Has anyone else had the same problem?

#stm32f401re-spi-keil-cubemx
This topic has been closed for replies.

2 replies

jasonp4113
Associate III
December 20, 2014
Posted on December 20, 2014 at 01:45

Hi

I have had this problem. Is seems to happen when you import a project generated by an earlier version of Cube.

The target device is still show as correct, but won't compile.

My workaround was to change the target device, exit the menu, re-enter the menu and then change the target back to what it should be.

Hope this helps.

Jason

stm32cube-t
ST Employee
January 9, 2015
Posted on January 09, 2015 at 10:52

Hello,

We don't reproduce your issue.

Have you used MDK pack installer to download latest pack for STM32 F4?

0690X00000605N0QAI.png