2018-07-13 1:03 PM
Hello community! I've got a problem with DMA and ADC (multi channel). I can't find solution why function
HAL_ADC_Start_DMA returns 0's to the 'adc_value' array. I have connected to Nucleo F466RE board 3 sensors, and i want to measure and get 3 values. Thanks for any prompts.
#include 'stm32f4xx.h'
#include 'stm32f4xx_nucleo.h'DMA_HandleTypeDef dma;UART_HandleTypeDef uart;uint32_t adc_value[3];
char result[20]='';int main(void)
{ HAL_Init();__HAL_RCC_DMA1_CLK_ENABLE();
__GPIOA_CLK_ENABLE(); __USART2_CLK_ENABLE(); __ADC1_CLK_ENABLE();GPIO_InitTypeDef gpioANALOG;
gpioANALOG.Pin = GPIO_PIN_0|GPIO_PIN_4|GPIO_PIN_1; gpioANALOG.Mode = GPIO_MODE_ANALOG; gpioANALOG.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOA, &gpioANALOG);GPIO_InitTypeDef gpioUART;
gpioUART.Pin = GPIO_PIN_3|GPIO_PIN_2; gpioUART.Mode = GPIO_MODE_AF_PP; gpioUART.Alternate = GPIO_AF7_USART2; gpioUART.Speed = GPIO_SPEED_HIGH; gpioUART.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOA, &gpioUART);uart.Instance = USART2;
uart.Init.BaudRate = 9600; uart.Init.WordLength = UART_WORDLENGTH_8B; uart.Init.StopBits = UART_STOPBITS_1; uart.Init.Parity = UART_PARITY_NONE; uart.Init.Mode = UART_MODE_TX_RX; uart.Init.HwFlowCtl = UART_HWCONTROL_NONE; uart.Init.OverSampling = UART_OVERSAMPLING_16; HAL_UART_Init(&uart);ADC_HandleTypeDef adc;
adc.Instance = ADC1; adc.Init.ContinuousConvMode = ENABLE; adc.Init.ExternalTrigConv = ADC_SOFTWARE_START; adc.Init.DataAlign = ADC_DATAALIGN_RIGHT; adc.Init.ScanConvMode = ENABLE; adc.Init.DiscontinuousConvMode = DISABLE; adc.Init.NbrOfConversion = 3; HAL_ADC_Init(&adc);ADC_ChannelConfTypeDef adcChannel;
adcChannel.Channel = ADC_CHANNEL_0; adcChannel.Rank = 1; adcChannel.SamplingTime = ADC_SAMPLETIME_480CYCLES; HAL_ADC_ConfigChannel(&adc, &adcChannel);adcChannel.Channel = ADC_CHANNEL_1;
adcChannel.Rank = 2; adcChannel.SamplingTime = ADC_SAMPLETIME_480CYCLES; HAL_ADC_ConfigChannel(&adc, &adcChannel);adcChannel.Channel = ADC_CHANNEL_2;
adcChannel.Rank = 3; adcChannel.SamplingTime = ADC_SAMPLETIME_480CYCLES; HAL_ADC_ConfigChannel(&adc, &adcChannel);dma.Instance = DMA1_Stream1;
dma.Init.Direction = DMA_PERIPH_TO_MEMORY; dma.Init.PeriphInc = DMA_PINC_ENABLE; dma.Init.MemInc = DMA_MINC_ENABLE; dma.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD; dma.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD; dma.Init.Mode = DMA_CIRCULAR; dma.Init.Priority = DMA_PRIORITY_HIGH; HAL_DMA_Init(&dma); __HAL_LINKDMA(&adc,DMA_Handle,dma);HAL_ADC_Start_DMA(&adc,(uint32_t*)adc_value,3);
sprintf(result,'ADC: %lu \n\r',adc_value[0]); HAL_UART_Transmit(&uart,result,sizeof(result),100); while(1) {}
}2018-08-09 8:39 PM
Does it wait for completion? Should DMA buffers be volatile.
Review examples under HAL/Cube trees