cancel
Showing results for 
Search instead for 
Did you mean: 

When the STM32WB06 is in the automatic connection enabled state, it is unable to enter the low power mode and the automatic connection fails aft

xxyyhhmm
Associate

Hi, I'm having some issues with the STM32WB06 when trying to achieve low power consumption. I hope someone can help me solve these problems.

Issue 1: After initializing the Bluetooth protocol stack and enabling automatic connection establishment, it causes the device to fail to enter the low power state (BLE wake-up has been disabled). Is this a normal phenomenon? If not, what are the solutions?

Issue 2: Before entering the low power mode, disabling automatic connection establishment allows the device to enter the low power mode normally. However, after waking up, attempting to re-enable automatic connection establishment fails (aci_gap_start_procedure(GAP_AUTO_CONNECTION_ESTABLISHMENT_PROC, LE_1M_PHY_BIT, 0, 0)). What is the solution for this problem?

xxyyhhmm_0-1779561009373.png

I look forward to your replies. Thank you very much!

0 REPLIES 0