cancel
Showing results for 
Search instead for 
Did you mean: 

Problem Uploading code to STM32F103ZCT7

krunal2411
Associate II
Posted on February 16, 2015 at 12:59

Hello all,

I am having problem in updating the code to STM32F103ZCT7 using ST link V2.

I am getting the error as ''Can not connect to divice; Internal Command Error''

I am using three pins SWDIO, SWCLK, NRST. 

I have cross check the connections using multimeter & all are OK.

I have not connected AVcc & AVss pins as well as Vbat pins i.e. they are floating, can this create any problem?

Please suggest.

Thanking You all.

#stm32f103zct7
3 REPLIES 3
Posted on February 16, 2015 at 14:23

Analogue supplies are not optional, they control the Power-On-Reset circuit.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
krunal2411
Associate II
Posted on February 17, 2015 at 04:20

Thanks Clive. I will power the analog part & will update here soon.

krunal2411
Associate II
Posted on February 18, 2015 at 13:30

Thanks Clive. 

Your suggestion worked for me.

:-)