2012-03-24 3:21 AM
Hello,
I just receive my STM32F4DISCOVERY. I installed IAR EWARM, and ST-Link driver V2. But after several tests on two laptops, I am unable to link the discovery board with ST-Link.This is the message displayed: ''Fatal error - ST-Link connection error Session aborded!''And this is the message on ST-Link utility: ''No ST-Link detected''Do you have any idea of what happened? Thanks!2012-03-24 3:44 AM
Ok I find the problem! IAR provided the ST-Link V2 driver, but it's not the latest version and it is not compactible with Windows Seven... Download ST-Link V2 driver on ST.com !
2012-07-26 6:02 PM
I find a short video about this problem which advices some ways to solving this problem. I was approached last piece of advice
Here is the Youtube Link