cancel
Showing results for 
Search instead for 
Did you mean: 

Problem resetting CAN after Bus Errors on STM32F446

GS1
Senior III

Hi all,

I have the problem concerning resetting the CAN bus after the other side was set to a wrong bitrate:

Example:

My system is sending data with 500 kBit. But the receiver is set to 1 MBit.

This results of course in Errors when sending data.

I handle this by resetting the CAN Bus port after a couple of Errors.

As soon as the receiver switches to the correct bitrate of 500 kBit, my system should then work properly, but it still gets Error Interrupts - even after another reset.

The debugger runs into "Error Warning" and "Error Passive" Interrupt states. And only a small part of the messages will be transmitted.

Sometimes it works as expected, but most times it is still getting Error Interrupts.

How can I safely return to a working CAN interface?

Here is what I do to reset the CAN Bus:

HAL_CAN_DeInit(&hcan1);

MX_CAN1_Init();   // Je nach Konfig aus SysInfo für Baudrate initialisieren

/* CAN1 init function */

void MX_CAN1_Init(void)

{

 hcan1.pTxMsg = &CANTxMessage;

 hcan1.pRxMsg = &CANRxMessage;

 hcan1.Instance = CAN1;

 hcan1.Init.Prescaler = 9;

 hcan1.Init.Mode = CAN_MODE_NORMAL;

 hcan1.Init.SJW = CAN_SJW_1TQ;

 hcan1.Init.BS1 = CAN_BS1_3TQ;

 hcan1.Init.BS2 = CAN_BS2_1TQ;

 hcan1.Init.TTCM = DISABLE;

 hcan1.Init.ABOM = ENABLE;

 hcan1.Init.AWUM = DISABLE;

 hcan1.Init.NART = DISABLE;

 hcan1.Init.RFLM = DISABLE;

 hcan1.Init.TXFP = DISABLE;

 if (HAL_CAN_Init(&hcan1) != HAL_OK)

 {

   _Error_Handler(__FILE__, __LINE__);

 }

}

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10

That is what I am seeing in FDCAN. I came upon a site where the termination was incorrect and noticed a protoype device (STM32G474) did not timeout and reconnect/continue to RX frames.

 

I am used to the PIC18 "classic-mode-CAN" which  will always have the error counters count back down and let the device try again. I shall perform some experiments and com up with a RESET FDCAN procedure that works for me.