2013-05-20 4:04 AM
Hi,
I need
to put my
card
STM32
-
P103standby
I
test the
consumption of all
the
card
I see that
it
uses up to
19mA
but
the literature indicates that
standby power
consumption must
be
to
some
uA
.here is my code
: #include ''stm32f10x.h'' #include ''stm32f10x_gpio.h'' #include ''stm32f10x_rcc.h'' #define LED_PORT GPIOC GPIO_InitTypeDef GPIO_InitStructure; ErrorStatus HSEStartUpStatus; void RCC_Configuration(void); void GPIO_Configuration(void); void main(void) { RCC_Configuration(); GPIO_Configuration(); PWR_EnterSTANDBYMode(); while (1) { } } void RCC_Configuration(void) { RCC_DeInit(); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB | RCC_APB2Periph_GPIOC | RCC_APB2Periph_GPIOD | RCC_APB2Periph_GPIOE | RCC_APB2Periph_AFIO, ENABLE); } void GPIO_Configuration(void) { GPIO_InitStructure.GPIO_Pin = GPIO_Pin_All; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_Init(GPIOB, &GPIO_InitStructure); GPIO_Init(GPIOC, &GPIO_InitStructure); GPIO_Init(GPIOD, &GPIO_InitStructure); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB | RCC_APB2Periph_GPIOD | RCC_APB2Periph_GPIOE, DISABLE); ADC_Cmd(ADC1, DISABLE); } and thank you for your help2013-06-26 4:54 AM
This might be better with a new thread as the board and part are different.
Current consumption relates to how much is turned off, the SLEEP mode really doesn't turn off much of anything, where as STOP does, and STANDBY significantly more.