2018-03-12 7:11 AM
In SPWF01S wifi module, could perform File system update using AT+S.HTTPDFSUPDATE over the air with the help of Apache web server successfully (from Lab6 of Wi-Fi Training - Hands On manual).
But the same is giving problem using UART
(from Lab6 of
Wi-Fi Training - Hands On manual)
after the below commands:• AT+S. HTTPDFSWRITE=357957
• In Tera Term: File – Send File...Not prompting to issue a reset command in order to complete the file system update, but hanging in the mid(PFA below). Please help me in solving this issue.
Thanks & Regards
Jitendra