2015-12-15 07:53 AM
Board
On board I found this file: FAIL.TXT - ''The interface firmware FAILED to reset/halt the target MCU''. Target>Settingshttps://yadi.sk/i/fblHZHiWmEfTm
https://yadi.sk/i/W4D_w54dmEfg2
I need
my own
firmware for
STlink/V2-1!where to get?
? #stm32f72015-12-15 10:19 AM
I need
my own
firmware for
STlink/V2-1!where to get?
?Google sayshttp://www.st.com/web/en/catalog/tools/PF260217
Though this might be more of a driver/dll issue, and you want to get current versions of those, along with the ST-LINK Utilities.If the problem persists you need to look at the power supply, and jumper settings about where the board is deriving power, because the messages suggest the F7 isn't running.The ''connect under reset'' settings look like they would address erant code, you could also try pulling BOOT0 high, after you have confirmed you have 3V available, and it's running the part.2015-12-16 12:39 AM
Hi, clivel!
I need afirmware
that
has been
the purchase.
https://yadi.sk/i/vP5xYaNtmG5Wh
where can I
get it?
Nowfirmware
https://yadi.sk/i/i41GXhc1mG47p
I'm
not the first
who uses
board
, so do notknow what to
do
with it
. It maybe a problem with
the stm32f7.
Unfortunately
no
conclusions
to
be connected
directly.
I hope you understand me.2015-12-16 05:35 AM
Hello,
As clive has said, it is clearly a power problem.So can you please check that jumper JP1 is in position 2 (5V link) and LD2 is onJust to understand:Your board already is Mbed enabled (embed STLink V2-1) as shown in thishttps://yadi.sk/i/fblHZHiWmEfTm
So why do you need to get STLink V2-1? and you already have it?even theFAIL.TXT :: ''The interface firmware FAILED to reset/halt the target MCU''
is shown within the MSD drive, which confirm that your board is with ST-Link V2-1
Then you have shown us another snapshot (the ST-Link Upgrade one) with V2J25S4, that is absolutely for STLink Standalone.Can you please clarify ?Regards,TarekB2015-12-16 09:10 AM
Your original screen shot shows V2J25M13, do you have multiple ST-LINK attached to your machine? Remove everything except the STM32F7-DISCO board. Make sure it is jumpered to use power from the on-board ST-LINK.
I've pointed at the current update file, it contains multiple images for different ST-LINK variants, it will not let you flash the Stand-Alone ST-LINK with the mbed ST-LINK/V2-1 firmware, they use a different F103 part.2015-12-16 09:16 AM
2015-12-20 09:40 PM
Hello.
Whenit was the standard
firmware
, the LED
light.
Firmware
V2J25S4
he
filled
, and
then update
it
.
It is possible that
problems with food
.
And I would like
zalist
standarntuyu
firmware
.
Not
in my
Dann
board
stopped working
, so I
probyval
different options.
There
drugana
fee
,
it
rabataet
.