STM32F030K6 Exit from sleep and stop mode
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-12-10 1:23 AM
Hi. Exit from sleep and stop mode not work. When STM32 in sleep mode and push to buttons on pins PA0, PA1, PA2, PA5, PA6, PA7, PA13 (low or high level) STM32 don't exit from sleep mode.
sleep_counter++; if((sleep_counter>=400000)&&(lamp_start==0)) { GPIO_ResetBits(GPIOF, GPIO_Pin_0); //A GPIO_ResetBits(GPIOF, GPIO_Pin_1); //B GPIO_ResetBits(GPIOA, GPIO_Pin_3); //C GPIO_ResetBits(GPIOB, GPIO_Pin_1); //D GPIO_ResetBits(GPIOA, GPIO_Pin_9); //E GPIO_ResetBits(GPIOA, GPIO_Pin_10); //F GPIO_ResetBits(GPIOA, GPIO_Pin_13); //G GPIO_SetBits(GPIOA, GPIO_Pin_14); //DP PWR->CSR = PWR_CSR_EWUP1 | PWR_CSR_EWUP2 | PWR_CSR_EWUP5 | PWR_CSR_EWUP6 | PWR_CSR_EWUP7; RTC_AlarmTypeDef RTC_AlarmStructure; RTC_SetAlarm(RTC_Format_BIN, RTC_Alarm_A, &RTC_AlarmStructure); RTC_ITConfig(RTC_IT_ALRA, ENABLE); RTC_AlarmCmd(RTC_Alarm_A, ENABLE); PWR_WakeUpPinCmd(PWR_WakeUpPin_1,ENABLE); sleep_counter=0; // Clear Wakeup flag PWR->CR |= PWR_CR_CWUF; // Select STANDBY mode PWR->CR |= PWR_CR_PDDS; // Set SLEEPDEEP bit of Cortex-M0 System Control Register SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk; // Request Wait For Interrupt __WFI(); }- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-12-10 11:28 PM
Exit from stop mode not work. On low or high level on pins PA0, PA5, PA6, PA7, PA13.
EXTI line is configured.//CWUF, PDDS and LPDS bits + SLEEPDEEP bit + WFIPWR->CR |= 0x07;SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;__WFI();How to exit from stop mode by low level on pin PA5.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-12-11 8:22 PM
Sorry, not using the F030 here, may be you can expand your presentation to provide more context to the code, and the board you are using it on?
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-12-15 4:03 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-12-20 10:50 PM
Solved:
void Configure_PA0(void)
{ /* Set variables used */ GPIO_InitTypeDef GPIO_InitStructure; EXTI_InitTypeDef EXTI_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; // Enable clock for GPIOA RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); // Enable clock for SYSCFG RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE); // Set pin as input GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); //GPIO_PinAFConfig(GPIOA, GPIO_PinSource0, GPIO_AF_0); // // Tell system that you will use PA0 for EXTI_Line0 SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOA, EXTI_PinSource0); EXTI_ClearITPendingBit(EXTI_Line0 | EXTI_Line1 | EXTI_Line2 | EXTI_Line3 | EXTI_Line4 | EXTI_Line5 | EXTI_Line6 | EXTI_Line7 | EXTI_Line8 | EXTI_Line9 | EXTI_Line10 | EXTI_Line11 | EXTI_Line12 | EXTI_Line13 | EXTI_Line14 | EXTI_Line15 | EXTI_Line16 | EXTI_Line17 | EXTI_Line18 | EXTI_Line19 | EXTI_Line20 | EXTI_Line21 | EXTI_Line22 | EXTI_Line23 | EXTI_Line25 | EXTI_Line26 | EXTI_Line27 | EXTI_Line31);/**/ // PA0 is connected to EXTI_Line0 EXTI_InitStructure.EXTI_Line = EXTI_Line0; // Enable interrupt EXTI_InitStructure.EXTI_LineCmd = ENABLE; // Interrupt mode EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; // Triggers on rising and falling edge EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising_Falling;//EXTI_Trigger_Rising_Falling; // Add to EXTI EXTI_Init(&EXTI_InitStructure); // �? �?°�?·Ñ€�?µÑˆ�?°�?µ�?¼ �?¿Ñ€�?µÑ€Ñ‹�?²�?°�?½�?¸Ñ� �?² �?¿�?µÑ€�?¸Ñ„�?µÑ€�?¸�?¸ �?´�?»Ñ� �?²Ñ‹�?²�?¾�?´�?¾�?² 0 EXTI->IMR |=(EXTI_IMR_MR0); // Add IRQ vector to NVIC // PD0 is connected to EXTI_Line0, which has EXTI0_IRQn vector NVIC_InitStructure.NVIC_IRQChannel = EXTI0_1_IRQn; // Set priority NVIC_InitStructure.NVIC_IRQChannelPriority = 0x00;//NVIC_InitStruct.NVIC_IRQChannelPreemptionPriority = 0x00; // Set sub priority //NVIC_InitStruct.NVIC_IRQChannelSubPriority = 0x00; // Enable interrupt NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; // Add to NVIC NVIC_Init(&NVIC_InitStructure); NVIC_EnableIRQ(EXTI0_1_IRQn); NVIC_SetPriority(EXTI0_1_IRQn,0);} DisableADC(); Configure_PA0(); sleep_counter=0; EXTI->FTSR = EXTI_FTSR_TR0; EXTI->IMR = 0; EXTI->EMR = EXTI_EMR_MR0; EXTI->PR = 0x0003FFFF; SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk; //PWR->CR &= ~(PWR_CR_PDDS|PWR_CR_LPDS); //PWR->CR |= PWR_CR_LPDS; PWR->CR |= 0x01; EXTI->PR = 0x0003FFFF; __NOP(); __WFE(); NVIC_SystemReset();