2008-02-27 10:05 PM
problem again with m24 memory with ev5
2011-05-17 3:25 AM
If I write 8 bytes in a row the debuging hangs at EV5 check.
Here is my code. I dont know what to do, If I go step by step it works. I have tried with I2C_DeInit(I2C1); at the stop command in the end but it dosent help. void I2C_EE_ByteWrite(u8 wByte, u8 WriteAddr) { u32 I2C_TimeOut = 0x3FFFF; int err = 0; while(err == 0) { // Check busy flag I2C_CheckEvent(I2C1, I2C_FLAG_BUSY); /* Send STRAT condition */ I2C_GenerateSTART(I2C1, ENABLE); /* Test on EV5 and clear it */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT)); /* Send EEPROM address for write */ I2C_Send7bitAddress(I2C1, 0xA0, I2C_Direction_Transmitter); /* Test on EV6 and clear it */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED) && I2C_TimeOut) { I2C_TimeOut--; } if(I2C_GetFlagStatus(I2C1, I2C_FLAG_AF) != 0x0) { err = 0; } else { err = 1; } } // Clear EV6 by setting again the PE bit I2C_Cmd(I2C1, ENABLE); // skicka adress till den minnesposition som data ska skrivas till (2ggr) /* Send the EEPROM's internal address to write to */ I2C_SendData(I2C1, WriteAddr); /* Test on EV8 and clear it */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); /* Send the EEPROM's internal address to write to */ I2C_SendData(I2C1, WriteAddr); /* Test on EV8 and clear it */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); // skriv data /* Send the byte to be written */ I2C_SendData(I2C1, wByte); /* Test on EV8 and clear it */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); /* Send STOP condition */ I2C_GenerateSTOP(I2C1, ENABLE); }