cancel
Showing results for 
Search instead for 
Did you mean: 

blocking downloading

per3
Associate II
Posted on March 04, 2008 at 10:39

blocking downloading

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
per3
Associate II
Posted on May 17, 2011 at 12:25

I have Raisonance RIDE 7. On the options there I see I can download the target code into a hex file.

This makes me wonder, is there some setting to do to prevevent this, just like they have in Atmelk AVR devices - you set a bit to block reading of the code.

Simply put, how do you prevent stealing of production code once you ship units?

jilisegiar
Associate II
Posted on May 17, 2011 at 12:25

Rlink configuration-> advanced options->click here to open option dialog box

and set the ''read out protection'' option then click on ''write target Option Bytes now'' button.