2025-09-21 11:21 PM
Hi everyone,
I’m working on an STM32 firmware project (HAL + CubeIDE). I’m trying to output debug messages to Tera Term via UART using printf and puts.
Here’s the situation:
Debug build: Both printf and puts work perfectly.
Release build: Calling printf or puts causes the MCU to reset immediately. Maybe due to watchdog reset and these function call cause the MCU freezing.
I also retarget the printf function by implemented the following:
int __io_putchar(int ch) {
while (!(huart1.Instance->ISR & USART_ISR_TXE));
huart1.Instance->TDR = (uint16_t)ch;
return ch;
}
int _write(int file, char *ptr, int len) {
for (int i = 0; i < len; i++) {
__io_putchar(ptr[i]);
}
return len;
}My questions:
Why do printf and puts crash/reset in Release but work in Debug?
Are there known issues with _write or __io_putchar in Release builds?
Any recommended approach to safely use printf/puts in Release firmware for UART output?
Thanks in advance!
2025-09-23 3:11 AM
Hi,
Sorry, I'm using STM32L071RZ, I think this series doesn't support semihosting.
Sorry, what is hardware flow control.
The UART initialization code is in below and it call before any printf and puts function.
void MX_USART1_UART_Init(void)
{
/* USER CODE BEGIN USART1_Init 0 */
/* USER CODE END USART1_Init 0 */
/* USER CODE BEGIN USART1_Init 1 */
/* USER CODE END USART1_Init 1 */
huart1.Instance = USART1;
huart1.Init.BaudRate = 115200;
huart1.Init.WordLength = UART_WORDLENGTH_8B;
huart1.Init.StopBits = UART_STOPBITS_1;
huart1.Init.Parity = UART_PARITY_NONE;
huart1.Init.Mode = UART_MODE_TX_RX;
huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart1.Init.OverSampling = UART_OVERSAMPLING_16;
huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART1_Init 2 */
/* USER CODE END USART1_Init 2 */
}it
2025-09-23 3:23 AM
> Sorry, I'm using STM32L071RZ, I think this series doesn't support semihosting.
Semihosting is not a MCU feature.
> Sorry, what is hardware flow control.
I highly suggest to take the time and read the USART/UART section of the reference manual of your MCU.
Especially in relation to asynchronous serial mode, event / interrupt handling, and register interface.
2025-09-23 3:33 AM
@chai2145 wrote:Sorry, what is hardware flow control.
That's where hardware signals are used by the connected devices to enable/disable the comms between them.
https://en.wikipedia.org/wiki/Flow_control_(data)#Hardware_flow_control
You disable it here:
huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;