2023-02-12 8:41 AM
So, I'm having an issue getting the printf() function suite to work with floating point values.
First, understand that I am not using STM32CubeIDE. It's a good tool, but I've had too many issues/complications using it. I use a custom Makefile and VScode for my development environment.
That said: With STM32CubeIDE I *can* go into the options and select "Use float with printf from newlib-nano (-u _printf_float)"
This adds "-u _printf_float" to the linker flags and floating point values work.
In My Makefile, I've added "-u _printf_float" to the linker arguments and floating point values are always "0.0".
I'm not sure what else would be causing this.
STM32's linker line versus mine:
arm-none-eabi-gcc -o "CT_ReadG431.elf" @"objects.list"
-mcpu=cortex-m4 -TSTM32G431KBTx_FLASH.ld
--specs=nosys.specs -Wl,-Map="CT_ReadG431.map" -Wl,--gc-sections -static --specs=nano.specs
-mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -u _printf_float -Wl,--start-group -lc -lm -Wl,--end-groupMine:
arm-none-eabi-gccm [Object list omitted for brevity] -mthumb -mfpu=fpv4-sp-d16 -mfloat-abi=hard
-specs=nano.specs -TSTM32G431KBTx_FLASH.ld -lc -lm -lnosys
-Wl,-Map=build/CT_ReadG431.map,--cref -Wl,--gc-sections -u _printf_float
-o build/CT_ReadG431.elfCould it be something else?
2023-02-14 5:02 AM
Well, as far as "buffer", that's how vasprintf() works..
"The functions asprintf() and vasprintf() are analogs of sprintf(3) and vsprintf(3), except that they allocate a string large enough to hold the output including the terminating null byte, and return a pointer to it via the first argument. This pointer should be passed to free(3) to release the allocated storage when it is no longer needed."
As for your other links... I will definitely read those and take them under advisement. I saw you had other posts with similar complaints so I can tell this is a sore spot for you!
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.