2020-09-20 7:37 AM
Following in the directions of this post, I am able to reserve and write to (and read back) from a section of FLASH dedicated to calibration data. However, when I reprogram the device, the IDE wipes the whole memory clean before programming and we lose all the data. Since we are in a debugging cycle, we are constantly reprogramming and have to write the calibration back as a first step every time. Is there a way to tell the IDE to only erase a certain region of memory corresponding to the program data? Thanks.
Modified linker memory definitions:
/* Memories definition */
MEMORY
{
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 1792K
TABLE (rwx) : ORIGIN = 0x81C0000, LENGTH = 128K
DATA (rwx) : ORIGIN = 0x81E0000, LENGTH = 128K
}
What we see when programming:
Erasing memory corresponding to segment 0:
Erasing internal memory sector 0
Erasing memory corresponding to segment 1:
Erasing internal memory sector 14
Erasing memory corresponding to segment 2:
Erasing internal memory sector 15
Download in Progress:
Solved! Go to Solution.
2020-09-20 8:17 AM
You should mark the section as NOLOAD.
https://mcuoneclipse.com/2014/04/19/gnu-linker-can-you-not-initialize-my-variable/
Another option would be to remove the section from your linker file and use a pointer to the user data. This has the benefit of not allowing the compiler to rearrange how it's storing things when you recompile the firmware.
2020-09-20 8:17 AM
You should mark the section as NOLOAD.
https://mcuoneclipse.com/2014/04/19/gnu-linker-can-you-not-initialize-my-variable/
Another option would be to remove the section from your linker file and use a pointer to the user data. This has the benefit of not allowing the compiler to rearrange how it's storing things when you recompile the firmware.
2020-09-20 8:29 AM
If there is data for the section in the .ELF, the tools will probably try to rewrite.
Use a NOLOAD / NOINIT section for stuff you don't want data in the .ELF / . AXF file.
Have your app write usable defaults, if you have multiple devices to debug, have a table driven by the unique ID
Keil doesn't write to unused sectors, it is a checkbox item in the debug/flash options
2020-09-20 1:34 PM
Thanks, to both of you. Adding (NOLOAD) was all it took. Learned something new today!
Cheers.