2012-06-01 01:59 AM
Dear all,
I need to design a board based on STM32F103RE.My board need to be powered in two ways, USB & Li-Ion 3.7V battery. In addition i need to design a IN-BUILT battery charging circuit( USB to Li-Ion battery) for the board. When I attach battery, it should be automatically charged and kept in this state until the other power source (USB or external adapter) is removed and it should AUTOMATICALLY power the board - no jumpers, no switches!I found the exact functional power_supply section in the following board schematics:OLIMEXINO-STM32 MAPLE / ARDUINO LIKE DEVELOPMENT BOARDhttp://www.olimex.com/dev/DUINO/OLIMEXINO-STM32/OLIMEXINO-STM32.pdf
http://www.olimex.com/dev/DUINO/OLIMEXINO-STM32/OLIMEXINO-STM32_Rev_B.pdf
This board has 3 power supply options. I need only two of them.I also have iNEMO v2 Board from ST Microelectronics :http://www.st.com/internet/evalboard/product/250367.jsp
It has two power supply options, but a switch is used to select one of them. Moreover, it needs 5V DC supply if USB power not used. In my case i want to use 3.7 Li-Ion/Li-Po battery when USB not used. I did not like the switch to select power source.I liked auto switching power source ofhttp://www.olimex.com/dev/DUINO/OLIMEXINO-STM32/OLIMEXINO-STM32.pdf
If it is possible to just remove the DC-DC power supply(power input voltage from 9 to 30V DC) part of OLIMEXINO-STM32 it really suits me.But i need to use SMD components to make my board as small as possible, like iNEMO v2.I would like to request if you have any suggestions for me or If you think you can solve my problem in few minutes & send circuit diagram, i will be very thankful.Below are the power management circuits of two boards i mentioned:Thank you. #stm32-power-management2015-09-17 04:53 AM
HI,
Did you suceed in implementing this?Any pointers to the folks here.2015-09-17 01:29 PM
We used an LTC4062
http://www.linear.com/product/LTC4062