cancel
Showing results for 
Search instead for 
Did you mean: 

Pointers on Designing TFT Based System for STM32H750XB

Caan
Associate III

Hello All,

               I need to design a board that will carry an IS42S32400F-6BL SRAM ,STM32H750XB MCU,Flash MT25QL512ABB1EW9-0SIT and Couple of support components along with Power supply.

My questions-

1) MCU Power Supply Protection

2) High frequency filter placements (ferrite beads)

3)SPI /I2C Pin protection

4) Analog and Digital Layers placement

5) Optimal PCB Layer to be used

6)PCB Stack  consideration

3 REPLIES 3
STTwo-32
ST Employee

Hello @Caan 

For some design tips on how to set your design using the STM32H750xB value line, you may want to start by refering to the Getting started with STM32H74xI/G and STM32H75xI/G MCU hardware development application note (AN4938). Also, you can refer to the design of the STM32H750B-DK since this board is based on the same MCU you will be using.

For a dedicated HW support, you may want to contact an HW expert to review your design and give you more advices dedicated for your case.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hey @STTwo-32,

                           Thanks for the support, But I am little bit confused on the series resistance that are placed between the SDRAM and MCU, In some places people are interfacing the STM32H750 without the series resistance as shown here.

Hello @Caan ,

There are no resistors between SDRAM data lines and the MCU. Only unused data lines are pulled low via pull down resistors:

mALLEm_0-1740143209783.png

This is because the SDRAM is used only in 16bit data width so the rest of the data lines D16 to D31 are unused.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.