2015-10-23 5:43 AM
Hi, is there any difference how exactly I'm getting the desired clock speed on SYSCLK through PLL? For example, let's say I want to have 48MHz on SYSCLK on STM32F407, using a 8 MHz HSE and the PLL. One way of doing it would be this:
HSE = 8MHzM = 8N = 384
P = 8
Q = 8
--------
SYSCLK = 48MHz Another way of doing it would this:
HSE = 8MHz
M = 4
N = 96
P = 4
Q = 4
--------
SYSCLK = 48MHz So my question is: is one of these two ways better than the other (i.e. lower jitter, or lower power consumption), and why? Thank you.
2015-10-23 1:54 PM
Obviously no, and the PLLs in various sub-families differ significantly from each other - for example, while in 'F4 the PLL input clock range is 1-2MHz, in 'F1 this range is 1-25MHz.
JW2015-10-24 4:26 PM
There are numeror bugs in CUBE that's why i only use it for pin mapping and even that dont work 100% depending device you are selecting and it has from the start and it is with the
latest release.