User Activity

Posted on June 05, 2017 at 16:19Will a default +5V 10k ohm pullup on swd/sck pins during prog/debug damage them?ST link firmware in the programmer seams to set up these pins as push-pullduring programming/debug.
Posted on November 09, 2015 at 23:48Concerns stm32f30x.h file and devices who uses it.
Posted on November 04, 2015 at 20:54Selecting alternate function graphics fig 27 page found in F42xxx/F40xx etc series is missing in F334 and F30x, AFRL and AFRH.
Posted on October 11, 2015 at 19:31In a function depending on ICF1F and IC1PSC beeing zero, no filter, no clock divide for a input capture to DMA request with input frequency of max 3-4 Mhz. DMA move byte data from memory to TIM CCR. Original appli...
Posted on October 02, 2015 at 17:02I want to write directly to DAC1,2,3 as i see them, DAC1 ch1, DAC1 ch2 and DAC2 ch1 as ref manual RM0316 describes, a voltage just as simple as writing to a TIM CCR is to output a voltage, like: TIM1->CCR1=120; so ...
Kudos from