cancel
Showing results for 
Search instead for 
Did you mean: 

please,To reduce internal RTC errors

HG LEE
Associate II
Posted on October 11, 2017 at 04:32

Hello, I am going to use the internal RTC. However, there are a lot of errors when using the internal RTC. I wonder if there is a way to reduce errors.I don't know because I'm a beginner. Thank you for giving me a detailed answer.

5 REPLIES 5
Posted on October 11, 2017 at 10:12

there are a lot of errors when using the internal RTC

What kind of errors?

Which STM32?

JW

Nesrine M_O
Lead II
Posted on October 11, 2017 at 12:25

Hi

qkqhsi159

,

1- What are you using as STM32 product?

2- What are exactly the problems you faced with RTC?

3-Could you please provide more explanation on your case, so that it will be easier to understand the issue?

-Nesrine

Posted on October 11, 2017 at 13:09

1-stm32f4007ig using

2.3-I would like to use internal rtc when I can't use external rtc.But I don't know how to hold the internal rtc.

       In short, I wonder if we can reduce the internal rate of internal error rates.

Posted on October 11, 2017 at 15:12

Read

http://www.st.com/resource/en/application_note/dm00025071.pdf

 

For precise timekeeping, you need to have connected a 32.768kHz crystal to the LSE oscillator pins, LSE enabled, and if you want to maintain time while the whole chip is powered down, you need to have a battery connected to VBAT.

JW

Posted on October 12, 2017 at 09:33

Dear

qkqhsi159

‌,

can you please share with us what errors you have? We would like to understand more what rates of errors you are talking about.

Thank you for your cooperation.

Best regards,

Tilen