cancel
Showing results for 
Search instead for 
Did you mean: 

Please provide a way to download older version of the cube.

Jnana Panuganti
Associate II
Posted on March 29, 2017 at 21:21

I recently upgraded to a new version, 4.20, and its has been giving us a lot of issues. Unfortunately I deleted 4.18 installer, Is it possible to provide a download link to an older version of the cube?

I am working on a commercial product and things like these are a big time sink for us.

This discussion is locked. Please start a new topic to ask your question.
42 REPLIES 42
Posted on April 02, 2017 at 19:29

That is true for the FW packages but not for the CubeMX itself, or I'm blind. For me it only lists the current 4.20.

Posted on April 03, 2017 at 10:50

Hi

Rudolf.Markus

The feature to archive older versions is not available for CubeMx.

Indeed, it is not possible to get back to an older CubeMx version unless you kept it on your computer.

So,don't hesitate to save CubeMX versions on which you worked to keepseveral versions.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Oleksandr Borysov
Associate II
Posted on July 15, 2017 at 19:23

Hello

I had problems with sources that CubeMX v4.21 generated for me and usage of older version helped me to solve the most of them. (The project at least compiled and show some working results)

I decided that this discussion can be a good place for the list of the previous CubeMX versions.

By the way, I recommend using the firmware package with CubeMX which was available during the release of the package. 

(CubeMX v4.18 with 

the firmware packages v1.14)

CubeMX v4.17 

https://drive.google.com/open?id=0B-9VDn2z6F3hb004NWxaTkV1ZFk

 

CubeMX v4.18 

https://drive.google.com/file/d/0B-9VDn2z6F3hQ3M1SV9ISkNqaGc/view?usp=sharing

 

CubeMX v4.21 

https://drive.google.com/file/d/0B-9VDn2z6F3hZk1KQnpTNExmUVU/view?usp=sharing

 

CubeMX v4.22 

https://drive.google.com/file/d/0B-9VDn2z6F3hVXNWaUZJTXQyMEE/view?usp=sharing

 

Storage: 

https://drive.google.com/drive/folders/0B-9VDn2z6F3hQVlta2wxNElXVlk?usp=sharing

 
Posted on November 20, 2017 at 18:58

I have a mirror of quite a number of CubeMX releases, and the libraries too. If you need something restartable due to internet outage or long down load times, I can probably post as a torrents.

ST's server performance seems to much better in recent weeks, so server/connectivity might have been changed or upgraded. I know Keil uses Amazon to host downloads.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on February 02, 2018 at 20:05

Hello Clive,

It seems that CubeMX 4.24 does not work well with TrueStudio v9.0.0, as mentioned in this post:

https://community.st.com/0D50X00009XkWopSAF

 

Would you happen to have the previous CubeMX v4.23 available for download?

That would be greatly appreciated.

Philipp

The new forum destroyed the link titles, so going to fix here, and see if the 3 link limit has been removed, click Show More to expand the post

v4.2.0 https://drive.google.com/file/d/0B7OY5pub_GfIbHZVV0RtN2hZUm8/view?usp=sharing

v4.4 https://drive.google.com/file/d/19ZunVFHvSQMZ6pvFlSabv8i1r8-HeQl9/view?usp=sharing

v4.9.0 https://drive.google.com/file/d/0B7OY5pub_GfIckg0RU5CdGlqTFU/view?usp=sharing

v4.10.0  https://drive.google.com/file/d/0B7OY5pub_GfIRC1oMEYtTTVfaTA/view?usp=sharing

v4.14.0 https://drive.google.com/open?id=1TRMT3gLebX0ymNjnXJwzrWjup-LJGIta

v4.15.0 https://drive.google.com/open?id=1NklqV8tGYvfTvoQZ9tM4T-yxfeyqFcyX

v4.15.1 https://drive.google.com/open?id=1F6meIlJRrnMPblBumeVyF0k_lRVvMQpQ

v4.16.0 https://drive.google.com/open?id=0B7OY5pub_GfINEVlT01sYzAxRU0

v4.17.0 https://drive.google.com/open?id=0B7OY5pub_GfId0NMdzVSeEhZT1E

v4.18.0 https://drive.google.com/open?id=0B7OY5pub_GfILUVZTXdKUkV6eU0

v4.19.0 https://drive.google.com/open?id=1KTdiPxQSgnhLnVZe7SeyutURmUpZaraq

v4.20.0 https://drive.google.com/open?id=0B7OY5pub_GfIdUxPaDl0ZFV3Q1k

v4.21.0 https://drive.google.com/open?id=1BCnG5z03V8mKEQmL76cecNUoI745a_fZ

v4.22.0 https://drive.google.com/open?id=1-9l-vPb35xm1kvOXxbOQrDKzTtPMnx22

v4.23.0 https://drive.google.com/open?id=0B7OY5pub_GfIbUYzWGZaU2dsRUE

v4.24.0 https://drive.google.com/open?id=1nclMp0ESduH4Y2B9cmKLpI3FAo9GUzgG

v4.25.0 https://drive.google.com/open?id=19ztTJrZvwQy-Hb4i3FwAk5yoR10nY63i

v4.25.1 https://drive.google.com/open?id=1ZuISNv5YHT7ZcnJeXOgYI3iZqE2wKjQm

v4.26.0 https://drive.google.com/open?id=1D702wAecmeYyZoBLzz25dPIBNwsFzvTG

v4.26.1 https://drive.google.com/open?id=1Jq3U0bTwpZ3hsOmOv6mkHlIjMuFID_qT

v4.27.0 https://drive.google.com/open?id=16uTm4TBdgU05XQyJPUvzOhC6aJWpqloa

v5.0.0 https://drive.google.com/open?id=1bA_wRq-p-m7KGlAy-KofRkRRUJ7godKj

v5.0.1 https://drive.google.com/open?id=1rQOLvuHWcVpOoWcw3qPzqF6WachrjiJi

If this post is helpful, please help maintain the mirror and my work here by contributing via PayPal or with Amazon Gift Cards - sourcer32@gmail.com

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on February 14, 2018 at 12:39

You wrote:

> So, don't hesitate to save CubeMX versions on which you worked to keep several versions.

No hesitation is involved. None at all.

You meant, I think:

> Always be mindful that when CubeMX updates, it could break. Therefore, keep your original CubeMX installation zip file, and thereafter each time you allow CubeMX to update, also log into the ST website and download that version of CubeMX. That way you'll have a means of returning to previous versions of CubeMX when you encounter a version that is broken beyond use. Furthermore, always backup your CubeMX projects before using a new version of CubeMX because *.ioc files written by a given version of CubeMX cannot be opened by previous versions. If you don't do this, then when you encounter a version of CubeMX that doesn't work, you are likely to lose all the projects that you (a) opened and saved, and (b) opened and recreated, with that version.

I hope that helps clarify the situation. Please let me know if I've got something wrong. It is based on my experience.

Please forward this message to the CubeMX developers (or a link to this thread) so that they know the trouble they are causing. I think it would help the Cube and CubeMX product quality if they saw things more from the user's viewpoint than they currently do.

Cheers,

JB.
Posted on February 14, 2018 at 13:05

'

they are causing'

I wonder how much of the burden should be on the cube developers, vs. users.

I mean it has to be crazy for anyone to use something so persistently invasive.

If a piece of software insists on automatically update, it better be near bug free. Otherwise, the user should have a say on if an update is to take place. 

Relying on buggy software that insists on automatically update is an expensive proposition, and a cost to development.

Jesus Villalobos
Associate II
Posted on June 21, 2018 at 02:10

Does anyone have a copy of cubeMX v4.15.1 ? 

Thanks

Posted on June 21, 2018 at 15:15

Yes. Try the link below.

https://drive.google.com/drive/folders/16Ly2E3Y14dnsgDetvuKv5h-TMYScRetq?usp=sharing