cancel
Showing results for 
Search instead for 
Did you mean: 

Please help me fix the error: Failure at line:6 in 'Target Software Scripts'. Please edit debug configuration setting. Cannot convert between character sets 'CP65001' and CP1252'. Thanks a lot!!!

YAn1
Associate
 
6 REPLIES 6
hroze.1
Associate II

Please help me fix the error:

Failure at line:6 in 'Target Software Scripts'. Please edit debug configuration setting.

Cannot convert between character sets 'CP65001' and CP1252'.

Thanks a lot!!!

Do the two machines have different keyboard settings?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
SBEN .2
Senior II

Hello @hroze.1​ ,

This seems like an encoding issue. Converting the file encoding might help you. Funnily enough, and because the file fits within Latin-1, you would be able to do that using Notepad++ by selecting the ANSI encoding and then saving the file:

0693W00000Bcc5YQAR.png 

Hope this helps.

Best regards,

@SBEN .2​ 

hroze.1
Associate II

I have the same problem

An old computer works without problems A new computer has the problem

I would appreciate if you could share with me how you solved the problem

Mhass.21
Associate

I had the same problem, the problem is not related to Atollic itself, we need to diable utf8 for worlwide language in Windows

0693W00000D2KWcQAN.png 

You are a genius. Thanks.

Ondrej