2015-11-06 3:55 AM
Hello.
My colleague is in trouble about NVIC of STM32L053.. At the moment, he wants to use several external interrupts; some of them are assigned to EXTI line 0, some others are assigned to EXTI line 1, and the rest are assigned to EXTI line2. According to him, EXTI line 0 doesn't work at all regardless edge trigger happens. Also some interrupts of line 1 and line 2 don't work at all regardless edge triggger happnes as well. Does he take care of setting register when he assigns several interrupt to the same vector ? If someone can offer a sample program to solve this issue, I appreciate it. Regards #n2015-11-06 5:13 AM
Perhaps if you show some code it might be more apparent why it isn't working.
What board is being used, and are the pins free/available?Is the SYSCFG peripheral enabled? What settings are written to the NVIC and EXTI? Can you read these registers back to confirm the settings, and those for the associated GPIO?