2025-06-20 6:02 AM - last edited on 2025-06-20 6:05 AM by Andrew Neil
Hi,
I want to know pinout to read flash from CHIP stm32F103zet6 using ST-LINK.
Can someone provide it, im new on STM32 chip.
Thanks.
2025-06-20 6:39 PM
Yeah I hope so, it will be not protected. Thanks for your information.
2025-06-20 6:42 PM
You will also be needing decoupling capacitors on all VCC/GND pair. And BOOT pins to select booting from FLASH or RAM and avoid the bootloader.
2025-06-20 6:44 PM
VBAT pin must also be at VDD level 3.3V
2025-06-20 6:45 PM
See BOOT0 and BOOT1 pin truth table in Reference manual.
2025-06-21 1:12 AM
As @avinash_elec says, you need a fully-functional design to be able to do this.
See the datasheet.
See also Application Note AN2586, Getting started with STM32F10xxx hardware development.