cancel
Showing results for 
Search instead for 
Did you mean: 

Pin function Spreadsheet

Stan0402
Associate II

Does ST provide an excel or CSV form of a pin functionality spreadsheet, to aid in assigning pin connections during development? This would be similar to Table 13 in the datasheet, but not in PDF form.

11 REPLIES 11
MikeDB
Lead

I exported the datasheet PDF to a Word file and then the pin assignments are in a table which is editable. It's a bit wonky in places but can be tidied up quite quickly and then exported to Excel. This is what I ended up with as I just wanted the SAI pins.

bmxk
Associate

I need this excel for STM32F407.