2013-08-23 06:06 AM
Hi everyone,
I overdrive the low-speed internal oscillator by external source with a small offset and small swing.Where can I find parameters for external clock(without bypassing LSI osc)?Thanks.Eugene #lsi #oscillator2013-08-23 06:39 AM
Not sure I understand, you should be able to supply an external clock for LSE of up to 1 MHz, but would need to set LSE bypass mode so as not to be driving OSC32_OUT.
Both LSI and LSE can be operated together, or separately.2013-08-23 07:12 AM
The oscillator is 32768 Hz. External and internal oscillators are working together.
I meant, is it possible to supply from external oscillator without bypass mode driving the OSC32_IN? If it is, where can I find signal parameters for OSC32_IN pin?Thanks